Technical FAQs

Ask a Question

Are the Wiggy testers NFPA70E certified?

Are the Wiggy voltage testers NFPA70E certified?

Product Line:
Obsolete Square D voltage testers.


Code Certification

The NFPA70E is the Standard for Electrical Safety in the Workplace. This Standard does not actually provide for certification of individual pieces of equipment. This is a Standard, not a certification document. The Wiggy`s are UL/CSA/ANCE certified.

Update:  The Wiggy line of voltage testers is obsolete and no longer available, no replacement. Consider another manufacturer for this product.

CTA-ID : 2033348
Was this helpful?
What can we do to improve the information ?