Technical FAQs

Ask a Question

Is it possible to order a Molded Case Circuit Breaker MAL36800 with factory installed optional lugs AL800MA7 instead of the AL900MA it usually comes with?

Use suffix 6468 to get AL800MA7 factory installed.

CTA-ID : 2033329
Was this helpful?
What can we do to improve the information ?