Technical FAQs

Ask a Question

Do the RLTB kits required for installation come with the 100% rated 2500A R frame breakers?

Yes, RLTB kits are included with 2500 A 100% rated circuit breakers.


CTA-ID : 2033310
Was this helpful?
What can we do to improve the information ?