Technical FAQs

Ask a Question

What are the repair parts for a QO342M200, Series S1, Load Center?<br /><br />

Only the parts listed below are considered field replaceable.
Cover - QOC342MF or QOC342MS
Interior Assembly - QO342M200I
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - KDL32200 (OBSOLETE and no longer available)
Main Circuit Breaker Connecting Strap - 4055901901 (3 req`d)
Main Circuit Breaker Connecting Strap Mounting Keps Nut - 2342702001 (3 req`d)
Indoor Cover Mounting Screw - 4020513002K (6 req`d)
Indoor Cover Door Hinge - 4028356450K (3 req`d)
Door Latch Kit - 4020284450K


CTA-ID : 2033355
Was this helpful?
What can we do to improve the information ?