Technical FAQs

Ask a Question

What are the repair parts for a SMS365W, Series E1 (E01)?

Only the parts listed below are considered field replaceable:
Complete Arc Suppression Assembly - 2 part numbers required:
Arc Suppressor Assembly (3 per switch) - 4052031850
Arc Shield (3 per switch) - 4052085601
Load Base Assembly (3 per switch, includes lugs) - 4052112050
Load Base Mounting Screw (3 required per load base) - 2142720241
Load Base Side Insulator (1 per load base) - 4052098601
Fuse Clamp Assembly per phase - line side - 4052031351 (two bolts included)
Fuse Clamp Assembly per phase - load side - 4052031350 (two bolts included)
Handle Knob Kit - 4028343550
Lug Assembly (per lug) - 4025128750
Lug Mounting Nut (per lug) - 2342702400



CTA-ID : 2033270
Was this helpful?
What can we do to improve the information ?