Technical FAQs

Ask a Question

Is there a lower limit on Micrologic breaker ratings that will work with the MDGF system?

The MDGF system will work on breakers with 400A sensor plugs and higher with GF settings down to 120A (0.3 of 400).

CTA-ID : 2034023
Was this helpful?
What can we do to improve the information ?