Technical FAQs

Ask a Question

What is the catalog number for a mounting foot for a QYU125 circuit breaker? Are they only available for QOU`s?

Use the QOU type mounting feet for these also. Use QOUMF1.


CTA-ID : 2034022
Was this helpful?
What can we do to improve the information ?