Technical FAQs

Ask a Question

What is the difference between 120/240 and a 240V rated QO breaker?

A 120/240 V breaker can only be applied on a system where the maximum voltage from any conductor to ground does not exceed 120V. A 240 V breaker can be applied on a delta system where the voltage to ground is 208 V, or where the transformer is not grounded.


CTA-ID : 2034015
Was this helpful?
What can we do to improve the information ?