Technical FAQs

Ask a Question

Why are 225A main breaker I-line panelboards HCN18652MN and HCN27742MN no longer available?

Issue:
Why are the HCN I-line panelboards obsolete and no longer available?

Product Line:
HCN I-line Panelboard

Environment:
Interior option for a I-line panelboard

Resolution:
Due to the pending obsolescence of K-frame breakers, which are used as the main breakers, these panelboards will no longer be offered.

See Digest Section 9 for current options.
Was this helpful?
What can we do to improve the information ?