Technical FAQs

Ask a Question

What is part number ULWCOM10016?

This is a jumper wire replacement kit for Masterpact NW UC1 and UC2 terminal blocks Z3, Z4 Z5, and T1 and T2 wiring points. See instruction bulletin 48049-560-01 for complete installation details. The kit includes 60 of these 2 inch long, tinned end jumper wires.

CTA-ID : 2034008
Was this helpful?
What can we do to improve the information ?