Technical FAQs

Ask a Question

What relay should be used for field installation of Form R6 on a Class 8903 Type LX contactor?

Issue:
What relay should be used for field installation of Form R6 on a Class 8903 Type LX contactor?

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
field install of relay needed

Resolution:
CA2SK11__ (insert voltage code). See Relays section of Digest for voltage code selection. The addition of a Class 9999 Type RLX bracket will allow for direct mounting of the relay to the contactor base plate.


CTA-ID : 2033745
Was this helpful?
What can we do to improve the information ?