Technical FAQs

Ask a Question

What is the catalog number for the shaft or push rod only for the external reset button XB5AA86102 used in LE1D metal enclosed starters?<br /><br /><br /><br />Customer called back and found LE1D18 on the starter he has. He needs the replacement shaft only for the reset button. He was given W404376362 and it is not a good catalog number. S. Glass<br />

The shaft or push rod is not available separately.



CTA-ID : 2033762
Was this helpful?
What can we do to improve the information ?