Technical FAQs

Ask a Question

What is the part number for replacement fuse clips used in a H362, Series F05, safety switch?

Issue:
Repair parts

Product Line:
Heavy Duty Safety Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Fuse clips are not available as an individual repair part. Please replace the complete Line Base Assembly, or Load Base Assembly, as appropriate.
Line Base Assembly = 4056603850
Load Base Assembly = 4056604050
Was this helpful?
What can we do to improve the information ?