Technical FAQs

Ask a Question

Is the old Masterpact M (IEC version) still available?

No, these are obsolete and NLA. The MP and MC versions (UL and ANSI) are still available as of 4/1/2007.


CTA-ID : 2033940
Was this helpful?
What can we do to improve the information ?