Technical FAQs

Ask a Question

<br />What the difference between the form F1, F3, B1and B3 on a XCSL566F1

F is 110vac This voltage is becoming obsolete and must convert to the XCSE when replacement is required. Only 24Vdc will be available in the XCSL solenoid devices.

B is 24vdc
1 is PG13.5 connector
3 is a 1/2`` npt connector



CTA-ID : 2033743
Was this helpful?
What can we do to improve the information ?