Technical FAQs

Ask a Question

<br /><br />What are the threads on the 80084150-013 tapped at the top float used with a 9035 float switch?

These dimensions are not available. The threaded piece that screws into the float comes with the 9049DCA2 and it is obsolete with no replacement.


CTA-ID : 2033730
Was this helpful?
What can we do to improve the information ?