Technical FAQs

Ask a Question

What the the dimensions of the XALD02 enclosure?

Issue:
What the  the dimensions of the  XALD02 enclosure?

Product Line:
Harmony Control Stations

Environment:
All Products

Cause:
Product Features

Resolution:
It is 4.17 inches High, 2.68 inches wide and 2.09 inches deep.


CTA-ID : 2033821
Was this helpful?
What can we do to improve the information ?