Technical FAQs

Ask a Question

What are the repair parts for the CH224N, series F5? (may be shown as F05)

The replacement parts for the CH224N, series F5 (F05) are as follows. No other parts are available.
Complete Line Base - 4056702950 (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line Base mounting screws - 40205-464-01 (requires 6 per line base)
Load Base Assembly - 40566-774-50 (requires one per phase - includes phynolic base, lugs and fuse clips)
Load Base mounting screws - 40205-464-01 (requires 2 per load base)
Arc Suppressor Assembly - 40539-220-01(requires one per phase)
Arc Suppressor mounting screw - 40205-145-01
Lug Assembly - 40251-162-51 (per lug)
Lug Assembly mounting screw - 21401-222-40
Switch Mechanism - 40566-786-50
Switch Mechanism mounting screws- 22999-405-62 (requires 2)
Handle Assembly - 40566-635-50
Lockplate - 40566-721-01
Lockplate mounting screws - 22999-405-62 (requires 2)
Neutral Assembly - CSN20 (Includes mtg. hardware and bonding screw)
Neutral Bonding Screw - Contact - Contact (888) SQUARED for further assistance.
Cover latch and spring - one each of 40566-072-01 (latch) and 40223-043-01 (spring)



CTA-ID : 2033680
Was this helpful?
What can we do to improve the information ?