Technical FAQs

Ask a Question

What is the suffix for adding copper mechanical lugs to the FA, FH, FC, FI, KA, KH, KC, KI, LA, LH, MA, MH, NA, NC, PA, PH, and PC breakers?

Order the breaker with the suffix ``8002``. Example: FAL361008002.

CTA-ID : 2033611
Was this helpful?
What can we do to improve the information ?