Technical FAQs

Ask a Question

What are the deadfront part numbers for an NF454L2 or NF454L2C interior?<br /><br />

Each panel will require the following:

(1) 80113-171-50 MLO Cover
(1) 80113-160-54 Branch Section
(1) 80113-175-50 Load End Cover





CTA-ID : 2033814
Was this helpful?
What can we do to improve the information ?