Technical FAQs

Ask a Question

What is the Terminal Lug Data for a CD324N General Duty Safety Switch?

The lugs on this device will accept (1) #6 AWG - 300 kcmil aluminum or copper conductors per phase. Although the lug will accept 300 kcmil conductors, the wire bending space available in the switch restricts the maximum to 250 kcmil conductors.


CTA-ID : 2032968
Was this helpful?
What can we do to improve the information ?