Technical FAQs

Ask a Question

What are the repair parts for a SU2040M200R Series M01?

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field replaceable:
Meter Cover Assembly - 4053442852
Meter Cover Assembly Mounting Screw - 4020513001K (This kit contains 10 screws, but only one is required to mount the cover)
Meter Sealing Ring - 2920910001
Main Breaker Cover Assembly - 4053446553 (Includes metal cover with integral thermoplastic cover)
Main Breaker Cover Sealing Screw - X1299
Main Breaker - QOM2200VH
Utility Pullbox Cover - 40534-381-52 (Includes hinges and utility sealing tab)
Utility Pullbox Cover Sealing Screw - X1299
Utility Pullbox Cover Mounting Rivets - (4) 2430315290
Meter Base Assembly - 4053446152 (Includes meter base, line and load side meter jaws, meter jaw blade guides and load side connector busbars)
Meter Jaw - (4) 4052706950 (OBSOLETE - REPLACED BY 7329794850) (Included in Meter Base Assembly)
Meter Jaw Blade Guide - (4) 4052761901 (Included in Meter Base Assembly)
Line Side (Utility) Phase Lugs - (2) 4025116251, Lug Mounting Keps Nuts (2) 2342702000
Line Side (Utility) Neutral Lug - 4025116051, Lug Mounting Keps Nut 2342702000
Load Center Cover - 7329491150 (Includes integral interior deadfront trim)
Load Center Cover Mounting Screws - 4020513001K (This kit contains 10 screws, but only 4 are required to mount the load center cover)
Load Center Interior Assembly - 7329490950 (Does not include load center interior main phase lugs nor (3) larger branch neutral lugs attached to the branch neutral bar. Does include load center interior main neutral lug)
Load Center Interior Mounting Screws - (7) 4020510001
Load Center Interior Main Phase Lugs - (2) 4025102451, Lug Mounting Keps Nuts - (2) 2342702001
Load Center Interior Larger Branch Neutral Lugs (attached to branch neutral bar) - (3) 4025130450
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 2032962
Was this helpful?
What can we do to improve the information ?