Technical FAQs

Ask a Question

Are 5kV 810A fuses available for HVL/cc switches?

Issue:
Are 5kV 810A fuses available for HVL/cc switches?

Product Line:
Medium voltage switchgear.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes. They must be ordered with the 1200A HVL/cc switch. The 810A fuses are 2-450E fuses in parallel. The part number for each fuse is 55GFMSJD450E. One switch will require 6 - 450E fuses.


CTA-ID : 2032816
Was this helpful?
What can we do to improve the information ?