Technical FAQs

Ask a Question

Can ground fault or other relays be used with medium voltage HVL/cc switches?

Overcurrent relays should not be used with switches in general. Undervoltage or phase unbalance relays are acceptable. Ground fault relays should not be used with a switch unless the ground fault current is limited to 400A by a grounding resistor. Relays can be used for indication only and not for tripping the switch.


CTA-ID : 2032814
Was this helpful?
What can we do to improve the information ?