Technical FAQs

Ask a Question

What is the ambient temperature rating for the 8910DPA contactor?

Per UL508, operating temperature range of the contactor is from 0 degrees C to 40 degrees C. These devices do also meet ARI standards.

CTA-ID : 2032815
Was this helpful?
What can we do to improve the information ?