Technical FAQs

Ask a Question

Can a PQ4606G plug-in unit be mounted horizontally - such that the long dimension of the plug-in unit is parallel with the busway?

The ``PQ`` type of busplugs only hang vertically. There is no fusible 60A unit available for horizontal mounting. Customer might be able to use the circuit breaker unit PFA34060GN, which hangs only 1 1/8`` below the bottom of the busway.


CTA-ID : 2032780
Was this helpful?
What can we do to improve the information ?