Technical FAQs

Ask a Question

What is the resistance between terminals on the neutral CT for the NW?

Resistance between T1 and T2 should be less than 100 Ohms.
Resistance between T3 and T4 should be in MegOhm range, or open.


CTA-ID : 2032932
Was this helpful?
What can we do to improve the information ?