Technical FAQs

Ask a Question

What are the repair parts for a CD323N Series F03 General Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Line base assembly - 40566-036-50
Load base assembly - 40566-028-50
Arc shield - 40566-019-01
Mechanism assembly - 40566-476-50
Handle assembly - 40566-103-50
Lockplate - 40566-058-01
Lug assembly - 40251-018-51
Neutral assembly - 40566-344-50
Base assembly mounting screws - 40205-151-01 (3) required for line base & (2) required for load base
Arc shield mounting screw - 40205-145-01
Neutral bonding assembly - Contact (888) SQUARED for further assistance.
Lockplate moungting screw - 22999-405-62 (2) required
Lug assembly mounting screw - 40205-142-02
Cover latch and spring - one each of 40566-072-01 (latch) and 40223-043-01 (spring)


CTA-ID : 2032903
Was this helpful?
What can we do to improve the information ?