Technical FAQs

Ask a Question

What is a SDM11VMB?

The SDM11VMB is a Square D Multi-Link Structured Wiring component. It injects a modulated input from a security camera, VCR, DVD or satellite antenna onto the RF signal from an bi-directional CATV system. It is a single channel combination modulator and b-directional amplifier. It is supplied with a Cat-5 input for the source to be modulated and a RG-6 coaxial cable input for the bi-directional CATV signal. A 120Vac power supply is included.


CTA-ID : 2032984
Was this helpful?
What can we do to improve the information ?