Technical FAQs

Ask a Question

Is SN400LA available in copper?

NO! It will accept copper or aluminum wire, but it is not offered in copper.


CTA-ID : 2032921
Was this helpful?
What can we do to improve the information ?