Technical FAQs

Ask a Question

What are the AIR ratings of a KHL, 600 Vac max. thermal-magnetic circuit breaker?

They are as follows:
at 240Vac = 65kA
at 480Vac = 35kA
at 600Vac = 25kA


CTA-ID : 2032788
Was this helpful?
What can we do to improve the information ?