Technical FAQs

Ask a Question

Can a MAL or MHL breaker be installed in a MA1000R enclosure?

Yes, this enclosure will accept both the MAL and MHL breakers (1000A Max.)
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 2032769
Was this helpful?
What can we do to improve the information ?