Technical FAQs

Ask a Question

What are the repair parts for a CD322N Series F01 General Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Line base assembly - 40566-420-50
Load base assembly - 4056002550K
Arc shield - 40560-018-01
Mechanism assembly - 40566-378-50
Handle assembly - 40566-387-50
Lockplate - 40566-388-01
Lug assembly - 40251-016-52
Solid neutral assembly - 40567-994-50
Base assembly mounting screw - 40205-160-01 (3) required for line base & (2) required for load base.
Arc shield mounting screw - 40205-145-01
Solid neutral assembly mounting screw - 40205-065-01
Neutral bonding assembly - Contact (888) SQUARED for further assistance.
Lockplate mounting screw - 22999-405-62 (2) required
Cover latch and spring - one each of 40566-072-01 (latch) and 40223-043-01 (spring)


CTA-ID : 2032768
Was this helpful?
What can we do to improve the information ?