Technical FAQs

Ask a Question

What are the repair parts for the CH221N, series F5? (may be shown as F05)

The repair parts for the CH221N, series F5 (F05) are as follows. No other parts are available.

Line Base Assembly -40566-422-50 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 40566-410-50 (requires one per switch)
Arc Suppressor Assembly - 40560-018-01 (requires one per switch)
Lug Assembly - 40251-016-52 (per lug)
Switch Mechanism - 40566-107-50
Handle Assembly - 4056684150K
Lockplate - 40566-376-01
Neutral Assembly - 40567-994-50
Neutral Bonding Screw - Contact (888) SQUARED for further assistance.
Line & load base mounting screw - 40205-160-01 (3 required for line & 2 required for load base assemblies)
Arc suppressor mounting screw - 40205-145-01 (1 required)
Lockplate mounting screw - 22999-405-62 (2 required)
Cover latch and spring - one each of 40566-072-01 (latch) and 40223-043-01 (spring)


CTA-ID : 2032880
Was this helpful?
What can we do to improve the information ?