Technical FAQs

Ask a Question

What is the AIC rating of our 8606 reduced voltage controller?

The 8606 is listed under UL file E70074. AIC ratings are 5kA for NEMA size 1 thru size 3, 10kA for sizes 4 and 5 and 18kA for size 6. This is true whether or not a circuit breaker or disconnect is installed with the starter.

CTA-ID : 2032878
Was this helpful?
What can we do to improve the information ?