Technical FAQs

Ask a Question

What is the termperature rating of the lugs for the Micrologic breakers?

They are suitable for 75 degree C cable. 90 degree C cable can be used but MUST be sized per 75 degree C cable.


CTA-ID : 2032912
Was this helpful?
What can we do to improve the information ?