Technical FAQs

Ask a Question

Can an FJA Circuit Breaker be replaced with an HJA Circuit Breaker in an I Line Panel?

Can an FJA circuit breaker be replaced with an HJA circuit breaker in an I-Line Panelboard?

Product Line:
I-Line panelboards sold and supported in the USA.

Cross Reference


Yes, however, the FJA Series, both 2 and 3 pole, requires 3`` of mounting space and the HJA, both 2 and 3 pole, will require 4.5`` of mounting space. Both meet 65k AIC. 

CTA-ID : 2032888
Was this helpful?
What can we do to improve the information ?