Technical FAQs

Ask a Question

Can a catalog number S29371 breaker fixed padlock attachment be installed without shutting off the circuit breaker?

The circuit breaker does need to be turned off for safety reasons when mounting this fixed padlock attachment. See document 48940-241-01.

CTA-ID : 2032700
Was this helpful?
What can we do to improve the information ?