Technical FAQs

Ask a Question

What tenant breaker was used in the EZ2BA?

This device accepted field installed QO or Q1 tenant breakers, 2-pole, 15-100A maximum. QO breakers were used for requirements from 15A through 70A (inclusive) and Q1 breakers were used for requirements from 70A through 100A (inclusive). Q1 breakers are no longer available but can be replaced by QO breakers.


CTA-ID : 2032637
Was this helpful?
What can we do to improve the information ?