Technical FAQs

Ask a Question

Is a flush cover available to replace the surface cover of a QO48M30DSGP generator panel?<br />What are the dimensions of the cover?

A flush cover, part number 4055310750 ,(obsolete and replaced by 4055345250) will physically fit on the device, but will also require 4 Cover screws, part number 4020513002K, to be purchased separately. No labels or stickers are included with the cover.
The height of the cover is 13.79 inches high by 10.41 inches wide.

CTA-ID : 2032562
Was this helpful?
What can we do to improve the information ?