Technical FAQs

Ask a Question

How can an outdoor HVL/cc lineup be lifted to the top of a building with a crane?

Issue:
How can an outdoor HVL/cc lineup be lifted to the top of a building with a crane?

Product Line:
HVLcc.

Environment:
Products sold in the United States.

Cause:
Assembly/ Installation.

Resolution:
Refer to Instruction Bulletin 6045-1, page 21. The HVL/cc outdoor sections are lifted from the bottom lifting eyes attached to the base channel. Spreader bars are required at the top to keep the lifting cables away from the exterior.


CTA-ID : 2032440
Was this helpful?
What can we do to improve the information ?