Technical FAQs

Ask a Question

What is the application temperature range for a 9013FSG2 pressure switch?

Issue:     
What is the application temperature range for a 9013FSG2 pressure switch?

Product Line:
Pressure Switches

Environment:
9013 Pressure Switches

Cause:
What is the application temperature range for a 9013FSG2 pressure switch?

Resolution:
Temperture Range is 0 degree F to plus 158 degree F


CTA-ID : 2032468
Was this helpful?
What can we do to improve the information ?