Technical FAQs

Ask a Question

What is the current rating for the ZB2BE101 and ZB2BE102 contact blocks?

Issue:
What is the current rating for the ZB2BE101 and ZB2BE102 contact blocks?

Product Line:
Harmony Push Buttons

Environment:
Harmony 22mm

Cause:
Product Specifications

Resolution:
They have a NEMA A600 rating of 10A continuous.


CTA-ID : 2032443
Was this helpful?
What can we do to improve the information ?