Technical FAQs

Ask a Question

What conduit hub provision are on the top endwall of a UTH7213T?

The ``T`` suffix of this catalog number indicated that this meter sockets top endwall is supplied with a hub opening, capable of accepting A-L type hubs. A-L type hubs are available for use with conduit from 2`` to 4``. Catalog number would be 2`` = A200L, 2.5`` = A250L, 3`` = A300L, 3.5`` = A350L, 4`` = A400L.

CTA-ID : 2032819
Was this helpful?
What can we do to improve the information ?