Technical FAQs

Ask a Question

Are the frames and mounting for the KI and KIL type circuit breakers the same physical size as the IK and IKL breakers they replaced?)

Yes. The two types of breakers have identical physical characteristics such as frame size, mounting holes, etc.

CTA-ID : 2032805
Was this helpful?
What can we do to improve the information ?