Technical FAQs

Ask a Question

Is the HOM816M200FTRB also available in a NEMA 1, indoor enclosure?

This particular design is only offered in a NEMA 3R, outdoor enclosure. This NEMA 3R loadcenter could be used in a NEMA 1 application, however.

CTA-ID : 2032445
Was this helpful?
What can we do to improve the information ?