Technical FAQs

Ask a Question

Can HVL/cc switchgear designed for bottom cable exit be modified for top cable exit?

Yes. Rear Extensions must be added to the back of the switchgear to provide extra depth. The standard rear extensions are 16.75``, 24.00`` and 30.00``.

CTA-ID : 2032436
Was this helpful?
What can we do to improve the information ?