Technical FAQs

Ask a Question

Can I use a NQ panel on 125VDC?

Issue:
Can I use a NQ panel on 125VDC?

Product Line:
NQ Panelboard

Environment:
Application

Cause:
Clarification

Resolution:
Yes, a single phase MLO NQ Panelboard can be used for 48VDC or 125VDC
The 125VDC QO/QOB breakers 15-30A @ 4KAIC, and  35-70A @ 10KAIC breakers, are self certified by Cedar Rapids.
A Main breaker can be also used as well if it has a 125vdc, or greater rating


CTA-ID : 2032388
Was this helpful?
What can we do to improve the information ?