Technical FAQs

Ask a Question

What contacts can be used in the XALD enclosures?

The ZENL1111 or ZENL1121 contacts will need to be used because they mount in the base of the enclosure. You can use ZB5 operators with the ZENL contacts in the XALD enclosures.


CTA-ID : 2032411
Was this helpful?
What can we do to improve the information ?