Technical FAQs

Ask a Question

What is a SDM81VC?

The SDM81VC is a modulator combiner hub. It has RG-6 coaxial cable inputs for up to eight modulators. The signals from all eight inputs are consolidated into a single RG-6 coaxial cable output. The output would feed the eight modulated signals to the modulator input of video distribution hubs SDM38VBIR or SDM38VHIR.

CTA-ID : 2032994
Was this helpful?
What can we do to improve the information ?